China Steel

Description

China Steel is a leading steel company in Taiwan. It has the longest conveyer belt for carrying raw materials to its destination. Covering a total length of 14km belt in their Kaohsiung plant in Southern Taiwan, HUS is adopted to monitor real-time operation with its 1,000 cameras 31 units of HUS-D4 network video recorder and 11 units of HJC-5000 network keyboard. Moreover, Honeywell’s fiber temperature sensor system is also integrated with HUS. Once the temperature raising alarm is received, HUS will trigger the corresponding TV wall, giving the end user the most accurate and efficient way to handle any emergency situation.